Technical FAQs

Ask a Question

What has replaced the obsolete 600A, 800A and 1000A EZM main breaker and main fusible switch units?

Issue:
Cross reference

Product Line:
EZM Mains

Cause:
Cross reference

Resolution:
Effective in May, 2016 the 600A, 800A and 1000A main units have been redesigned and are now provided with PowerPact circuit breakers or molded case switches. Please refer to the attached handout 4141HO1601 for cross referencing to the new catalog numbers. 
Was this helpful?
What can we do to improve the information ?