Technical FAQs

Ask a Question

Are the 9001KR16 compatible with the hermetically sealed contact blocks?

Issue:
9001KR16 to hermetically sealed contact block compatibility

Product Line:
9001K Operators

Environment:
Pushbutton

Resolution:
No. They're not compatible. There's a tab on the 9001KR16 adapter which fits the slot on normal 9001 contact blocks. Hermetically sealed contact blocks don't have the slot for it.
 
Was this helpful?
What can we do to improve the information ?