Technical FAQs

Ask a Question

What are the means of accessing/connecting to the individual devices in a smart system?

There are two ways:
            1.  Utilizing Modbus/TCP to connect to SCADA, Cloud, BMS, or other systems.
            2.  Access and display on a PC via LAN
 
Was this helpful?
What can we do to improve the information ?