Technical FAQs

Ask a Question

Does Schneider Electric offer a H365RB Heavy Duty Safety Switch?

Issue:
Does Schneider Electric offer a H365RB Heavy Duty Safety Switch?

Product Line:
Heavy Duty Safety Switches

Environment:
NEMA 3R, Fusible, 3 Pole, 600V, 400A 

Cause:
Customer asking for the RB bolt-on Hub provision.

Resolution:
H365RB is not a valid catalog number. The B suffix indicates a bolt on hub provision is provided in the top end wall. That provision is only available on Type 3R switches through 200A. We offer the H365R for NEMA Type 3R. The top end wall will be blank. 

Was this helpful?
What can we do to improve the information ?