Technical FAQs

Ask a Question

Can the XVC1B3K, 100mm (4 inches) diameter Tower Light be broken down in components?

Issue:
Can the XVC1B3K, 100mm (4 inch) diameter Tower Light be broken down in components?

Product Line:
XVC, 100 mm Diameter Tower Light

Environment:
XVC Tower Lights, 100 mm diameter (4 inches), base mounting, without buzzer, with LED flashing or steady light, 24Vdc, R,O,G

Cause: 
Customer wants to cut the lead time. 

Resolution:  
No, the XVC1B3K come pre-wired, components are not available.  
Was this helpful?
What can we do to improve the information ?