Technical FAQs

Ask a Question

How can the version of software used to program a SR2 or SR3 relay be determined?

Issue:
How can the version of software used to program a SR2 or SR3 relay be determined?

Product Line:
Zelio Logic Relay- GIC Product

Environment:
US Product

Cause:
Product Specifications

Resolution:
Simply press the menu/ok button and scroll up or down until version is displayed.  Press the menu/ok button again and all of the information about the unit will display.
 
Was this helpful?
What can we do to improve the information ?