Technical FAQs

Ask a Question

Please elaborate on how the ground switch will be for fixed-type switchgear? I know that for withdrawable type switchgear, we usually get a ground switch bucket that we can use to ground specific feed

The market requires a visible disconnect. In withdrawable switchgear, this is accomplished by removing the breaker from the connected position. In fixed mounted switchgear, the visible isolation is accomplished via the use of a disconnect switch.
  • The grounding switch in Schneider Electric's HVL/cb switchgear has an optional feature.
  • The grounding switch in Schneider Electric's newest "Premset" offer is always provided.
Each of these offers have the ability to ground the load side of a feeder. 
Was this helpful?
What can we do to improve the information ?