Technical FAQs

Ask a Question

How do i upgrade the firmware of a Conext SW/XW/XW+ using the Conext ComBox?

Please download the attached Conext Series of Devices - Firmware Update Guide and follow the following steps

1) Step 1 - Read safety, overview, scope and requirements information
2) Step 2 - Upgrade the ComBox Firmware
3) Step 3 - Upgrade Xanbus Device using the ComBox via the ComBox Configuration | Upload option. 

Please note that the ComBox will need to be powered via the supplied AC/DC power adapter or a stable 24VDC power supply via the RS-485 connector. The ComBox will also require a network router as it requires a DHCP enabled router which is capable of DNS Name Resolution. Additionally high Xanbus traffic can impact the ComBox's ability to successfully upgrade the firmware of selected Xanbus Device. 
Was this helpful?
What can we do to improve the information ?