Technical FAQs

Ask a Question

What options are available for firmware upgrade of Conext SW/XW/XW+ Battery Based Inverters?

A firmware upgrade of Conext SW/XW/XW+ battery based inverters can be performed via the following devices and their software

1) Conext ComBox - part number 865-1058

2) Conext Configuration Tool - part number 865-1155-01

Schneider Electric recommends the use of the Conext Configuration Tool were possible as the ComBox requires a stable 24VDC power supply and can be affected by Xanbus network traffic
Was this helpful?
What can we do to improve the information ?