Technical FAQs

Ask a Question

XVUC29P

Issue:
What is the Luminous Intensity of the XVUC29P?

Product Line:
Stack Lights

Environment:
XVU Stack Lights

Cause:
Product Characteristics

Resolution:
Although this value will impacted by a lot of factors such as Angle, Direction, ambient brightness, distance...etc, the unimpeded values can be seen below:

 
 
Part: XVUC29, Direction of measurement : 90 Degrees
Color   Luminous (cd/cm2)
Red      321 ~ 351
Green 432 ~ 462
Blue     98 ~ 128
Yellow 366 ~ 396
Orange            220 ~ 250
White 190 ~ 220

 
Was this helpful?
What can we do to improve the information ?