Technical FAQs

Ask a Question

What does the PKGTALP2 ground bar kit contain?

Issue:
Product Features

Product Line:
Load Centers

Cause:
Clarifiying  

Resolution:
The PKGTALP2 contains (1) PK9GTA and (1) PK18GTA with an LK100AN lug installed on the PK18GTA (leaving only 15 terminals available on the PK18GTA, and mounting screws.  
Was this helpful?
What can we do to improve the information ?