Technical FAQs

Ask a Question

Does the SC816F200PS have feed through lugs?

Issue:
Product Features

Product line:
Homeline Combination Service Entrance Devices

Cause:
Clarification of product design features

Resolution:
Yes, the SC816F200PS is supplied with load side feed-thru-lugs, for #4vAWG - 250 KCMIL Al/Cu conductors. 
Was this helpful?
What can we do to improve the information ?