Technical FAQs

Ask a Question

What circuit breakers can be used in the JD250S

Issue:
Application

Product Line:
Circuit Breaker Enclosures

Cause:
Application

Resolution:
The JD250S is UL listed ONLY to accept a HDL or JDL, 3-Pole, 80% rated circuit breakers. The voltage is limited to 480Vac maximum. The SCCR is limited to 18K rms symmetrical amperes at 240Vac or 480Vac. Copper conductors (75 Degree C) MUST be used (aluminum conductors are not acceptable).


 
Was this helpful?
What can we do to improve the information ?