Technical FAQs

Ask a Question

How to Mount Contact Blocks to a 9001 30mm Operator

Product Line:
9001K and 9001SK Operators


Resolution:
Make sure no nearby components are powered during the installation.
1. Allign the contact block with either the plastic base piece or the light module base.
2. Use a small, flathead screw driver and tighten the mounting screw on the contact
Was this helpful?
What can we do to improve the information ?