Technical FAQs

Ask a Question

Video: How to Mount a Harmony XB5/ZB5 22mm Operator Push Button

Product Line:
Harmony XB5/ZB5 22mm Operators

Make sure you don't have power to any component during the installation.

1. Take your operator and insert it into the 22mm hole facing the outside.
2. Press the mounting collar firmly to the base of the operator head from the inside of the enclosure. Make sure that the arrow on the collar aligin swith the arrow on the operator head. You should hear a snap when it is attached.
3. Attach any contact blocks/lighting module by insterting the bottom plastic nub, and then press the contact until the metal hooks attach to the back of the collar.

Was this helpful?
What can we do to improve the information ?