Technical FAQs

Ask a Question

How to Install a Latching Mechanism to a 8501XO Relay

Product Line:
8501XO Relays

Resolution:
Always first make sure that power has been removed from the device.
1. Remove the face plate off of the relay
2. Attach the thin black plastic piece that holds the rod
3. Attach the rod to the base via the small white plastic part.
4. Slide the mechanism on the rod.
5. Press down on the open area underneath the piston to all the rod to fully passthrough
6. Enjoy the usage of your latching relay
Was this helpful?
What can we do to improve the information ?