Technical FAQs

Ask a Question

Video: How should the components be installed onto the XVU tower/stack light base?

Product Line:
XVU Tower
XVU Stack Light
XVU Sounder Unit

Resolution:
To install you will take the unlock on either side of the sounding unit or the light module and line that up with the arrow on the base unit. Once attached, turn the light/sounder to the locked position. If this is the last/top unit be sure to attach the cap to the top of the tower. It will follow the same practice of lining up the unlock sign to the arrow.



Was this helpful?
What can we do to improve the information ?