Technical FAQs

Ask a Question

What are the lugs rated on H600SNC and H600SN?

Issue: 
What are the lugs rated for on H600SNC and H600SN? 

Product Line: 
PTCCB-MCCBS, EARTH LEAK AND SWITCH 

Environment: 
Product Features 

Cause: 
Lugs rating

Resolution
The H600SN will accept (4) #1 - 750kcmil Al/Cu wire PLUS (1) #4 - 300kcmil Al/Cu Service Ground.
The H600SNC will accept (2) #1 - 600kcmil Cu and (2) #4 - 350kcmil Cu PLUS (2) #6 - 250kcmil Cu Servicee Ground.

 
Was this helpful?
What can we do to improve the information ?