Technical FAQs

Ask a Question

How to fix the cabin air filter event 4046 on an XCNA?

Issue:
Cabin air filter event 4046 on XCNA

Product Line:
XCNA

Environment:

Causes:

Loose connections

Resolution:
Note: The work instruction provided is meant for those who are qualified to work on the inverter. This means that they should know how to properly Lock out and Tag Out (LOTO) the inverter...,etc.

There are two thermo switches in the inverter to monitor the cabinet temperature, TS1 and TS2. They are located in the AC and DC cabinets. Please see the attached picture to show one of them that came loose. It is located right next to the QS2.
Was this helpful?
What can we do to improve the information ?