Technical FAQs

Ask a Question

What is the life expectancy on LC1SKGC200U7?

Issue;
What is the life expectancy on LC1SKGC200U7?

Product Line;
LC1SKGC200U7

Environment;
Contactor

Cause;
Life Expectancy

Resolution;
It is 10 million cycles/ 1200 cycles per minute.
 
Was this helpful?
What can we do to improve the information ?