Technical FAQs

Ask a Question

What is the horsepower rating of HU366, HU366R, HU366AWK, HU366DS or HU366SS safety switch?

Issue:
Application

Product Line:
HD SS

Cause:
Need hoursepower rating for application.

Resolution:
These 600A, 600Vac/600Vdc maximum safety switches are rated for 200 HP at 240Vac three phase, 400 HP at 480Vac three phase, and 500 HP at 600Vac three phase. They are also rated for 50 HP at 250Vdc or 600Vdc. The HP ratings applicable for a safety switch are printed on the Wiring Diagram, located inside the front cover of the switch.
Was this helpful?
What can we do to improve the information ?