Technical FAQs

Ask a Question

Equalization with multiple units

Issue:

Customers would like to know if they should equalize with inverter connected to grid/generator, or with charge controllers, or both

Environment:

Conext system with XW/SW and MPPT

Resolution:

Inverter with generator is preferred, and will override charge controllers if both are active
When using charge controllers, ensure that solar will remain stable for the entire hour required
Equalization should be done only as often as recommended by your battery manufacturer

Cause:

N/A
Was this helpful?
What can we do to improve the information ?