Technical FAQs

Ask a Question

Can an alternate ampere rated breaker be installed in the SC2040M200F CSED All-In-One?

Issue:
Application

Product Line:
CSED

Cause:
Alternate main breaker

Resolution:
Yes, the factory installed 200A QOM2200VH can be removed and replaced with a lower ampere rated QOM2-VH main breaker:
100A = QOM2100VH
125A = QOM2125VH
150A = QOM2150VH
175A = QOM2175VH
Was this helpful?
What can we do to improve the information ?