Technical FAQs

Ask a Question

CLNA - AC OC err Service Alarm Code: 2450

Criterion:
AC current measured in  one phase is above (Over Current) the  limit 
 
Possible cause :
 Can be external or internal issue
 
Action :
If this problem is not cleared automaticaly and observed frequently then replace the inverter - Collect the units fault logs 
Was this helpful?
What can we do to improve the information ?