Technical FAQs

Ask a Question

CLNA - AC init flt & AC BIST flt Service Alarm Code: 205&206

  • Criterion:
  • the initialization of the AC control processor failed
  • Built in Self Test of the AC control processor failed
  • Possible cause :
  • Firmware bug
  • Action :
  • Turn off and on both DC switch and AC breaker
  • If failure persists upgrade the firmware 
Was this helpful?
What can we do to improve the information ?