Technical FAQs

Ask a Question

CLNA - Other faults

Early firmware may throw nuisance events at boot or at end of day
Cycling BOTH PV and Grid usually clears the faults
Check for availability of Firmware updates
If the following faults do not clear and are not attributed to site conditions, device generally requires replacement


http://solar.schneider-electric.com/product/conext-cl-na-solar-inverter/
Was this helpful?
What can we do to improve the information ?