Technical FAQs

Ask a Question

CLNA - AC low temp Service Alarm Code: 2060

  • Criterion:
Temperature on AC power modules is lower than limit Temp – 25°C 
  • Possible cause :
 - very low external temp
- Internal circuit detection issue
  • Action :
- Wait until external ambiant temp get higher and the inverter will start.
Was this helpful?
What can we do to improve the information ?