Technical FAQs

Ask a Question

Why is my Conext CLNA showing an alarm code: 4700 (Low Power Wrn Service Alert)?

Issue: 
Customer is calling to confirm alarm code: 4700 (Low power wrn Service Alert).

Product Line: 
Conext CL 18000NA Conext CL 25000NA

Environment:  
On site troubleshooting

Resolution:  
Thumb screw should be inspected for the correct torque value.
Please see the attached picture.
 
Cause:
4700 Low power wrn - The input PV power is low. The unit does not go online and recovers when sufficient input power is available.
Was this helpful?
What can we do to improve the information ?