Technical FAQs

Ask a Question

Can we have a dongle or a hardware protection on a SoMachine project?

Issue:
Protect a SoMachine project or library with a dongle

Product Line:
Controllers (PLC & PAC) for Industrial machines

Resolution:
You need to buy a security USB key (Dongle) from the Codesys store, plug it in your laptop then open SoMachie and go to:
Project > Project Settings > Security and Enbale project file encryption and select Dongle.
The dongle should be detected and you will need to add it to the project (See attached photo).

Here is the link to buy the Dongle:
http://store.codesys.com/codesys-security-key-standard.html
Was this helpful?
What can we do to improve the information ?