Technical FAQs

Ask a Question

Do Homeline circuit breakers meet 240.81 of 2008 NEC for "indication?"

Issue:
Do Homeline circuit breakers meet 240.81 of 2008 NEC for "indication?"

Product Line:
Homeline circuit breakers sold and supported in the USA.

Environment:
Code

Cause:
Specification

Resolution:
Homeline circuit breakers do meet 240.81 of 2008 NEC for "indication." The indicator flag on the QO circuit breaker product line is an additional feature not required by the NEC. 
 
Was this helpful?
What can we do to improve the information ?