Technical FAQs

Ask a Question

Do we have a Surgelogic TVSS Device rated for use in 400 Hz Applications?

Issue:
Do we have a Surgelogic TVSS Device rated for use in 400 Hz Applications?

Product Line:
Surgelogic product line

Environment:
Application

Cause:
Selection

Resolution:
No, all Surgelogic devices are only rated to be used on 50/60 Hz applications. 
 
Was this helpful?
What can we do to improve the information ?