Technical FAQs

Ask a Question

Are lugs included on the 9422TG disconnect switches?

Issue:
Are lugs included on the 9422TG switches or do they have to be ordered separately?

Product Line:
Flange mounted disconnect switch

Environment:
Class 9422 Type TG1, TG2, unfused, fused  400A

Cause:
Are lugs included?

Resolution:
Per GIC Help Files, yes they are included.

Replacement lug for 9422TG is 25050-448-06.
Was this helpful?
What can we do to improve the information ?