Technical FAQs

Ask a Question

What are the repair parts for an EZM31200FSB, Series M01 main fusible switch unit?

Current design repair parts

Product Line:
EZM Metering

Repair parts


Only the parts listed below are considered field replaceable:

Top Cover assembly - EZM31200FSBTC (cover assembly includes one handle, breaker cover door/box and all appropriate labels)
Bottom cover assembly - 7329386376 (cover assembly includes one handle and latch) 
Cover Screws - 4020513002K (this is a bag of 10 cover screws, the top cover uses 2 and the bottom cover uses 4)
Top Cover Sealing Screw - X1299 (top cover uses 2)
Main Molded Case Switch - PJP36000S12
Bonding Strap Kit  - 7329696760 
Wall Mounting Channel - 7329354303
End Closing Cap Kit - EZMCAP (Left Side)
End Closing Cap Kit (Right Side ONLY Shallow) - EZMSCAP

NOTE: For alternate lugs see CAD drawing #PWFDS-SYTI-0032 in the 2D CAD system on-line)

Was this helpful?
What can we do to improve the information ?