Technical FAQs

Ask a Question

Solid State Relay Ratings in Digest 177

Issue:
Are the Solid State Relay Ratings correct in Digest 177?

Product Line:
Solid State Relays - GIC Product

Environment:
US Product

Cause:
Product specifications

Resolution:
The load current range ratings listed for the SSRP relays on page 23-36 of Digest 177 are incorrect.  The correct ratings are as follows and will be corrected in future online corrections:

SSRPCDM12D5 - 12A
​SSRPCDM25D5​ - 25A
​SSRPCDM40D5 - 40A
​SSRPCDS10A1 - 10A
​SSRPCDS25A1 - 25A
​SSRPCDS50A1 - 50A
​SSRPCDS75A2 - 75A
​SSRPCDS90A3 - 90A
​SSRPCDS125A3 - 125A
​SSRPP8S10A1 - 10A
​SSRPP8S25A1 - 25A
​SSRPP8S50A1 - 50A
​SSRPP8S75A2 - 75A
​SSRPP8S90A3 - 90A
​SSRPP8S125A3 - 125A

http://download.schneider-electric.com/files?p_Doc_Ref=0100CT1501_SEC-23
Was this helpful?
What can we do to improve the information ?