Technical FAQs

Ask a Question

Will the QO40M200 load center accept the QO2DTIM mechanical Interlock?

Issue:
Application
 
Product Line:
QO Load Center
 
Cause:
Application
 
Resolution:
It will depend on the application. 
For a generator application to interlock the factory installed main breaker to a generator backfed breaker, use QOCGK2C.
For an application requiring that only one two branch breakers can be ON at a time, use QO2DTI.
The QO2DTIM would be used if both breakers are being backfed and only one breaker can be ON at a time.    
Was this helpful?
What can we do to improve the information ?