Technical FAQs

Ask a Question

What is the length of the shaft for the RE10 Door mounted opemch for the H, J and L frame breakers?

Issue:
What is the length of the shaft for the RE10 Door mounted opemch for the H, J and  L frame breakers?

Product Line:
Powerpact Accessories

Environment:
Application

Cause:
Clarification

Resolution:
The shaft dimension has a range of 7.7" -23.5" from the back of the breaker to the front of the enclosure door 
Was this helpful?
What can we do to improve the information ?