Technical FAQs

Ask a Question

What is the part number for the phenolic strips with horizontal permanent numbers for the NQ 42 and 84 circuit panels ?

Issue:
Circuit Identification

Product Line:
Panelboards

Environment:
NQ

Cause:
Labelling

Resolution:
80110-190-09 is for the  strip numbered 1-41 .80110-190-10 is for strip numbered 2-42. These 1/4"w strips have black letters on white background and are mounted vertically on the deadfront . Two screws are provided. Number strips for 43-84 horizontal would be (2)80110-192-05SPL engraved as 43-83 and 44-84 ODD.

Was this helpful?
What can we do to improve the information ?