Technical FAQs

Ask a Question

PJA36080CU44A: What is the C designation in the part number, and the difference without the C?

Issue:
What is the C designation, and difference without the C for the I-Line Powerpact breakers?

Product Line:
Panelboards, Powerpact P and R frame

Environment:
Powerpact P and R frame breaker

Cause:
Full 100% rated breaker

Resolution:
The Powerpact P or R frame breakers with the C in the 9th character space designates 100% rated. Breakers without the C would be the standard 80% rated.  EX:  PJA36080CU44A is 100% rated

Was this helpful?
What can we do to improve the information ?