Technical FAQs

Ask a Question

What is the wire range for the HCP18686M panelboard ?

Issue:
What is the wire range for the HCP18686M panelboard ?

Product Line:
I Line Panelboard

Environment:
Application

Cause:
Wire sizing

Resolution:
The Main breaker for the Interior will accept (2) 4/0-500 kcmil conductors per phase , reflecting  NEC Wire bending restrictions
See current Digest 177 page 9-54 link below:

http://download.schneider-electric.com/files?p_Doc_Ref=0100CT1501_SEC-09
Was this helpful?
What can we do to improve the information ?