Technical FAQs

Ask a Question

What are the cover part numbers for RWT06TE and RWTR06EE Wall duct?

Issue:
What are the cover part numbers for RWT06TE and RWTR06EE Wall duct?

Product Line:
Wall Duct

Environment:
Maintenance

Cause:
Replacement

Resolution:

Catalog no.    Cover Only        List Price Ea.
RWT06TE    45206-678-02        $84.00
RWR06EE    45206- 624-51        $84.00
PE10 discount.  These covers will not system price.
Est. leat lime is 2-3 weeks 
*Tinnerman Speed Nut  is P/N: 23303-01100 Qty (4) needed
*Cover Plate Screw is P/N: 45102-407-01 Qty (4) needed
  * These part numbers are System recognized for pricing

 
Was this helpful?
What can we do to improve the information ?