Technical FAQs

Ask a Question

Can a 9001KSK be used outdoors ? Is in Nema 3R rated ?

Issue:
Outdoor rating for 9001K key-operated selector switch

Product Line:
Push Buttons

Environment:
30mm, 9001K

Cause:
Application

Resolution:
No. There are no boots or covers available either . 
Was this helpful?
What can we do to improve the information ?