Technical FAQs

Ask a Question

What are the repair parts for the H361, series F5? (may be shown as F05)

Issue:
Repair Parts

Product Line:
HD Safety Switch

Cause:
Maintenance

Resolution:
The replacement parts for the H361, series F5 (F05) are as follows. No other parts are available.

Line Base Assembly - 4056642050 (requires one per switch. Arc suppressor assembly not included)
Load Base Assembly - 4056002550 (requires one per switch)
Arc Suppressor Assembly - 4056669451 (requires one per switch)
Lug Assembly - 4025101652 (per lug)
Switch Operating Mechanism - 40566-107-50
Handle Assembly - 4056684150K
Lockplate - 4056637601
Line & Load base mounting screw - 4020516001 (3 for line & 2 for load)
Arc Suppressor mounting screw - 4020514501 (1 required)
Lockplate mounting screw - 2299940562 (2 required)


CTA-ID : 10005
Was this helpful?
What can we do to improve the information ?