Technical FAQs

Ask a Question

Are there weathershields for the EX tranformers 225KVA, 300KVA and 500KVA?

Issue:
Are there weathershields for the EX tranformers 225KVA, 300KVA and 500KVA?

Product Line:
EX Transformers

Environment:
Application

Cause:
Product selection

Resolution:
The weathershields are provided Factory assembled for the 25J enclosure style for the 225KVA. 300KVA and 500KVA EX tranformers , rating them Nema 3R from the Factory.
See Digest 177 link below:

http://download.schneider-electric.com/files?p_Doc_Ref=0100CT1501_SEC-14
Was this helpful?
What can we do to improve the information ?