Technical FAQs

Ask a Question

What is the terminal lug data(or wire range) for the EZM31600GCBC?

Issue:
Standard Terminal Lug Data

Product Line:
EZM Metering

Environment:
EZM Main Breaker lugs

Cause:
Standard terminations

Resolution:
The EZM31600GCBC will accept as standard (6) 1/0 to 750Kcmilj OR (12) 1/0 to 250kcmil AL/Cu wires per phase and neutral and (1) # 6 - 300kcmil Al/Cu wire per ground lug.  SEE THE CAD DRAWING #PWFDS-SYTI-0007 FOR OPTIONAL LUGS

Was this helpful?
What can we do to improve the information ?