Technical FAQs

Ask a Question

What is the bus rating of the RC816F200C, RC816F200CH CSED Meter-Main?

Issue:
Application

Product Line:
CSED

Cause:
Clarification of ratings

Resolution:
The bus rating is equal to the maximum main breaker rating: 200 Ampere. 
Was this helpful?
What can we do to improve the information ?