Technical FAQs

Ask a Question

What is the difference between XUSLDSY5A0760 and XUSL4E30H076NS1/S2?

Issue;
What is the difference between XUSLDSY5A0760 and XUSL4E30H076NS1/S2?

Product Line;
Light Curtain

Environment;
Hand Protection Light Curtain

Cause;
Part Difference

Resolution;
The XUSLDSY5A0760 is a Hand Protection light curtain used as a "slave" unit requiring an XUSLDM "master unit."
The XUSL4E30H076NS1/S2 are both Hand Protection Light curtains used as "slave" units to a required XUSL4  NM "master" unit.  The S2 "slave" unit connects to the "master" unit, and the S1 "slave" connects to the S2 "slave" unit.



 
Was this helpful?
What can we do to improve the information ?