Technical FAQs

Ask a Question

Is there a handout or something that shows the Old Homeline catalog numbers and the New Plug-On Neutral catalog numbers?

Issue:
Product design features

Product Line:
Homeline Load Centers

Environment:
New Plug-On Neutral load center catalog numbers.

Cause:
Needing new Plug-On Neutral catalog numbers

Resolution:
A handout showing the old Homeline catalog numbers and the new Plug-On Neutral catalog numbers is document number 1170HO1402. If you google this number the document should show up.
Was this helpful?
What can we do to improve the information ?