Technical FAQs

Ask a Question

Will HCW68D door kit fit on the 4 piece trim of HCWM326812N?

Issue:
The HCW68D door kit is not fitting on I-Line panel HCWM326812N.  It is short by 1/2 inch.

Product Line:
I Line Panelboards

Environment:
Maintenance

Cause:
Old style I Line Panel

Resolution:
The current door kit, HCW68D will not fit on the older I-Line 4 piece trims.  There is no available door kit.
Was this helpful?
What can we do to improve the information ?