Technical FAQs

Ask a Question

Can you order a stainless steel enclosure only for an existing mini power zone?

Issue:
Replacement SS enclosure for MPZ

Product Line: 
LV Transformers

Environment: 
 Mini Power Zone

Cause:
Specifications for MPZ products sometimes require stainless steel enclosures

Resolution: 
No, we do not provide replacement enclosures for the MPZ devices at all. And, even if we did, the nameplate would not reflect the change to stainless steel and that would be a UL Listing and labeling problem.

 
Was this helpful?
What can we do to improve the information ?