Technical FAQs

Ask a Question

Can SoMove create a log file of the captured data points over time?

Is SoMove software capable of generating a log file of capture data points?
Product Line:
SoMove software

All released  versions as of 9/15/15
Information unavailable in current literature.

No, SoMove software can not create a log file of captured data.  The Oscilloscope function can be used to capture data points but it can not generate a log file to track the data points over an extended period of time.   

Was this helpful?
What can we do to improve the information ?